Other Parts Discussed in Thread: DIR9001, PCM1794, PCM1794A, PLL1708, TS3L110
Hi,
Im planning to feed my PCM1794A with I2S data. I want to switch the I2S Signal with an 74HC157D 2-input multiplexer. As far as I see the PCM1794 uses the clock source from the I2S Signal. Now when I switch the Sources the Clock also changes. Is that a problem or do I have to use one clock Source for all the devices (DIR9001 and PCM2707)?
Is it possible to use a "master clock", for example the PLL1708, to generate a master clock Signal for the whole I2S Net?
How do I have to supply this clock? Using the SCK0 Output from the Clock Source and supply it to all BCK inputs?
regards
Patrick