Hi,
I would like to use LMK04808 Pll but I can't understand if mode Single Pll, External VCO, 0-delay is available. From datasheet (pag.6, 0-Delay Single Pll paragraph) I've read this phrase: "It is also possible to use an external VCO in place of PLL2's internal VCO", but in Device Mode Selection (pag.29) I can use Pll2 (Single Pll), 0-Delay only with internal VCO. In case this modality is available, could you suggest me how can I set it?
Thanks in advance.