Is there an Updated Model? The neither output will work if inverting outputs are selected in Hyperlynx. Both work if non inverting is selected. Need model asap!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there an Updated Model? The neither output will work if inverting outputs are selected in Hyperlynx. Both work if non inverting is selected. Need model asap!
Hi Craig,
This may not be an issue with the IBIS. Page 27 of the datasheet describes that the Negative side can only be enabled if the Positive side is enabled
http://www.ti.com/lit/ds/symlink/cdcm6208.pdf
Regards
Arvind Sridhar
Set the inverting differential output to a non complementary output in hyperlynx and output works.
Set the inverting differential output to a complementary output in hyperlynx and output fails.
Same thing happens on non inverting output. Need solution asap as it is critical to release a new design.