Hi!
Our customer will use LMK04828 device in RRH system.
So, Out customer want review of TI.
Also, I will recommend SN65LVEP11 instead of ICS85311 in 1:2 Fanout Buffer.
How about your think?
Please review attached schematic file.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
Our customer will use LMK04828 device in RRH system.
So, Out customer want review of TI.
Also, I will recommend SN65LVEP11 instead of ICS85311 in 1:2 Fanout Buffer.
How about your think?
Please review attached schematic file.
You can recommend CDCLVP1102 for the 1:2 fanout buffer since it has much lower additive jitter than SN65LVEP11.
Here are my comments on the schematics of LMK04828:
- On outputs where LVDS signaling level is desired, it is better to configure outputs as LVDS and then use 100 ohm between P and N before AC coupling capacitors. You save more power this way. If SYSREF can be LVDS, please follow the same as above as well.
- Use a pulldown on SYNC pin. This sets a default known state on the pin.
- The loop filters are reversed. What is noted as PLL1 loop filter is for PLL2 and what is noted as PLL2 loop filter is for PLL1. Please correct these.
- The power supply design is not optimal. It is better to isolate Vcc_CP2, Vcc_VCO, Vcc_PLL1, Vcc_PLL2, Vcc_DIG, Vcc_OSCin and Vcc_OSCout from rest of supplies using ferrite beads. You can group Vcc_VCO, Vcc_PLL1, Vcc_DIG using a ferrite bead (followed by an array of 10uF, 1uF, 0.01uF). You can group Vcc_PLL2, Vcc_CP2 using a ferrite bead (followed by an array of 1uF, 0.1uF, 0.01uF). You can group Vcc_OSCin and Vcc_OSCout using a ferrite bead (followed by 1uF, 0.1uF, 0.01uF). On output supplies (Vcc_CG[0-3]), please group them together and use a 1uF for each supply (total of 4). Please follow user guide for recommendations on supply network.