Other Parts Discussed in Thread: LMK04906
Hi,
I tried to launch the LMK04906 EVB but it seems that the PLLs don't lock. I can program different output clocks via the uwire interface, so in general the system seems to work. But looking on the LD_TP the PLL1/2 DLD signals are on ground. The PLL1_R/2 signal shows half the Phase Detector Frequency as expected. I also tried to use different high accuracy input clocks.
Strange to me is that the VCC VCXO_TP is on ground, too.
Thanks in advance,
Maximilian