This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can CDCLVD2108 input be driven with a differential CMOS output?



I have a clock signal from a CMOS  flip-flop with differential outputs (Q and !Q) I would like to connect these directly to both inputs of the clock buffer.The supply voltage of the flip-flop and the clock buffer is the same at 2.5V.

The app note only shows a single output to input, with the other input pin connected to a fixed DC voltage level, so I would like to be sure. Thanks.