Other Parts Discussed in Thread: LMK04826, LMK04826BEVM, CODELOADER
Hello All,
I am using codeloader4 in order to generate a jitter free clock and the evaluation module used for this purpose is LMK04826B. Consider, I am able to generate a clock of the desired frequency with the default settings in the SYSREF and Others tab. Giving an input to the CLKin1 tab I am able to see the lock on both PLL's 1 and 2.
What I want to know now is how to improve the clock generated (with no jitter) using the SYSREF tab. If I don't change settings in the SYSREF tab (i.e., with the SYNC mode operating) and change only the digital delay, analog delay and clock divider values in CLKOuts or Distribution tab, is it sufficient? I am trying the read the chapter 5 from the manual (http://www.ti.com/lit/ds/symlink/lmk04826.pdf) but I am not able to understand completely because there are many variables which I am not able to find in the CodeLoader4 software. I want to enable SYSREF (section 5.3) and want to know its significance.
Please can anyone help to understand the functioning of this SYSREF?
Best Regards,
NP.