Other Parts Discussed in Thread: CDCM61002
I just wanted to confirm that the recommended connection for a 3.3V LVCMOS input clock is to DC-couple it. The SCAA111 application report does not mention using a 3.3V input at all. Why is the recommendation in the datasheet for 2.5 V LVCMOS to use AC-coupling and 3.3 V LVCMOS to use DC coupling? Wouldn't DC coupling cover both?