Hello All,
I used Clock Design tool and based on the attached screenshot values generated 500 MHz clock from LMK04826BEVM. I can see 500MHz with a duty cycle of 51.9% in a DCA.
When I connect the output of DCLKOut0 to SSA, I can see that the phase noise measurement is around 150ps which is not good since in the documentation I can see we can achieve phase noise around 100fs. Please can anyone suggest if there are any ways to improve my phase noise?
Best Regards,
NP.