I want to use the CDCM61001 to generate a 66.67MHz LVDS clock signal. From using the equation on page 2 and table 3 "Table 3. Generic Configuration" on page 11. I see that I will need an input crystal with a frequency of 26.664MHz. Will a crystal with a frequency of 26.65MHz be sufficient or will I need to find a crystal that exactly matches the calculated value?