This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVP1204 - The maximum value of tRJIT

Other Parts Discussed in Thread: CDCLVP1204

Hello,

My customer has a question about CDCLVP1204.

[Q]

Please tell me the maximum value of tRJIT.

I understand that it is not a guarantee value.

<TEST CONDITIONS>

fout=25MHz

Vin=Single ended or differential

Integrated offset frequency = if it is possible 12kHz to 5MHz, (10kHz to 20MHz)

Regards,

Hiroshi Katsunaga