This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE925 Configuration

Other Parts Discussed in Thread: CDCE925

Dear application team,

Can you check if the configuration file bellow can be applicable to CDCE925 and
obtain 66MHz and 124MHz clock from 16MHz input (Xtal resonator) ?
I want to try it but I do not have CDCE925 EVM in my hand.

Mita

Bit => 7 6 5 4 3 2 1 0
Byte0 0 0 0 0 0 0 0 1
Byte1 0 0 0 0 0 0 0 0
Byte2 1 0 1 1 0 1 0 0
Byte3 0 0 0 0 0 0 1 0
Byte4 0 0 0 0 0 0 1 0
Byte5 0 1 0 1 0 0 0 0
Byte6 0 1 1 0 0 0 0 0
Byte7 0 0 0 0 0 0 0 0
Byte8 0 0 0 0 0 0 0 0
Byte9 0 0 0 0 0 0 0 0
Byte10 0 0 0 0 0 0 0 0
Byte11 0 0 0 0 0 0 0 0
Byte12 0 0 0 0 0 0 0 0
Byte13 0 0 0 0 0 0 0 0
Byte14 0 0 0 0 0 0 0 0
Byte15 0 0 0 0 0 0 0 0
Byte16 0 0 0 0 0 0 0 0
Byte17 0 0 0 0 0 0 0 0
Byte18 0 0 0 0 0 0 0 0
Byte19 0 0 0 0 0 0 0 0
Byte20 0 0 0 0 1 1 0 1
Byte21 0 0 0 0 0 0 1 0
Byte22 0 0 0 0 0 0 0 0
Byte23 0 0 0 0 0 0 0 0
Byte24 1 1 1 1 1 1 1 1
Byte25 1 1 0 0 0 1 1 1
Byte26 1 1 0 0 0 0 1 0
Byte27 0 0 0 0 0 1 0 1
Byte28 1 0 0 1 1 1 1 1
Byte29 1 0 1 1 0 0 0 0
Byte30 0 0 0 0 0 0 1 0
Byte31 1 0 0 0 1 0 0 0
Byte32 0 0 0 0 0 0 0 0
Byte33 0 0 0 0 0 0 0 0
Byte34 0 0 0 0 0 0 0 0
Byte35 0 0 0 0 0 0 0 0
Byte36 0 1 1 0 1 1 0 1
Byte37 0 0 0 0 0 0 1 0
Byte38 0 0 0 0 0 0 0 1
Byte39 0 0 0 0 0 0 0 1
Byte40 1 1 1 1 0 1 1 0
Byte41 0 0 0 1 0 0 0 0
Byte42 0 0 0 0 0 0 1 1
Byte43 1 1 1 0 1 0 0 0
Byte44 1 0 0 1 1 1 1 1
Byte45 1 0 1 1 0 0 0 0
Byte46 0 0 0 0 0 0 1 0
Byte47 1 0 0 0 1 0 0 0