Other Parts Discussed in Thread: LMK03806, LMX2581, SN74LV8154, LMK04828
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMK03806, LMX2581, SN74LV8154, LMK04828
Hi Saurabh,
Perhaps you are looking for a GHz clock? LMK03806 and LMX2581 are possible candidates.
Regards
Arvind Sridhar
Thanks Arvind for a quicky.
to measure 1 ns time interval can u suggest how should I use these in the circuit i mean what should be other components.
Can this be used for measuring time for single bit transfer between two wireless devices which are 10 cm away.
Arvind,
Diclosure: I'm a hobby guy, not an EE. My idea can become commercial, but I have to prove the concept first :-)
I too need a nano (or sub-nano) second timer.
I was thinking a 10Ghz clock (or 2Ghz at least) into a 16 or 32 bit counter.
I found sn74v8154 but the datasheet (http://www.ti.com/lit/ds/symlink/sn74lv8154.pdf) says the clock duration min to be 10 nano seconds. and all the other counters I looked at had even higher mins.
This seems like I'm making the simple complicated, but is there already an IC which counts nano seconds (or some other ultra small time slice)?
I also thought of 555 timer, but again, I can't find a counter fast enough to handle nano second clock.
Where to go from here?
Russ
Hi Russ,
My team does not support 555 timers and counters. However, we do have a device LMK04828 which support an external input of 3 GHz on Fin and cascaded (1-8191) and (1-32) dividers
Regards
Arvind Sridhar
Wow!
I was asking for a fly swatter and you give me an M1-Abrams tank!
I'm fully confident that this would work for me (and NASA), but did I mention I'm a hobby kinda guy and not an Electrical Engineer?
So have I asked for something that does not exist or do I need to roll-my-own for this one?
Should I go to another forum?
Russ
Hi Russ,
Best to continue searching in other TI forums :-)
Regards
Arvind Sridhar
Hi Tuan Vu Phan,
LMK04828 device supports SPI interface for register programming.
Regards
Arvind Sridhar