All the outputs of CDCE925 are set to 16MHz-only, and the measure is looked for.
Please look at attachment for details.
I have the following ideas. Although a host writes a slave address (1100100) to CDCE925 first about the waveform of SDA and SCL, an acknowledge does not return from CDCE925.
Is it right although having given the command suddenly considers the cause?
(The 9th shot of SCLK thinks that CDCE returns an acknowledge by Low)
Does below have a problem then?
-Start condition is NG.
-A device is different.
-The SDA drive by the side of a host.
-etc
Best regards,
Satoshi