This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Getting DS110DF410 to lock at 11.049Gbps

Other Parts Discussed in Thread: DS110DF410

Hello!

We are using a DS110DF410 in a new application.  We are successfully using it at OC-192 (9.953Gbps) and 10GbE, however, we would like to run the device at 11.049Gbps.

I am having trouble figuring out the register values that I will need to program correctly.  In reading the data sheet, it looks like for 11.049Gbps, that would make Nppm = 14143 or so, or 0x373F in hex.  I believe that is the value I should put in both registers 0x60, 0x61 and 0x62, 0x63.  Is that a correct calculation?

However, I am not sure what I need to put into register 0x2F, as the only reference for these values is table 1?  Should I select the highest data rate from the table, or is there a method to calculate the value for 0x2F based on the data rate.

Thanks!