Other Parts Discussed in Thread: CDCM7005-SP
Hi Team,
We are supporting one of our customer with CDCM7005-SP. They want to use CDCM7005-SP as clock buffer. The input of the Buffer will be fed at VCXO input and buffered to five outputs.
The input Fed to VCXO input is 75Mhz sine wave and is 2Vpk-pk.
I was looking in the datasheet for a minimum slew rate spec on VCXO input lines but couldn't fine so. Instead rise time spec was mentioned. Which as per the calculation for 75Mhz sine wave comes out to be 2.67ns for 20% to 80% which is within the datasheet spec of 3ns. Will this work for sine wave input?
Please let me know if this fine or any issues can arise because of sine wave input?
Thanks and Regards,
Robin Gupta.