HI! all,
My customer wants to know the default value of all registers of LMX2581 when RESET bit of REG5 is set or power is turned on.
Regards,
Toshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Toshi,
The power on defaults for this device arethe device in Partial Powerdown (LDOS powered up, rest of the chip powered down) and with outputs off. Specifically, the Default Settings are as follows:
R15: 0x0200 080F
R14: 0x0010 000E
R13: 0x4082 410D
R12: 0x0000 000C
R11: 0x0000 000B
R10: 0x2100 200A
R9: 0x0000 0009
R8: 0x2000 0008
R7: 0x0008 2317
R6: 0x0000 04C6
R5: 0x0000 0065
R4: 0x0000 0004
R3: 0x200A 0833
R2: 0x0C00 0002
R1: 0x0000 0011
R0: 0x002A 0000
Regards,
Dean