Hi,
Does anyone has information on this DDR4 RDIMM part MTA36ASF2G72PZ-2G1A2, if control/address mirroring is used or not? This part has raw card B.
Thanks,
Kin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kin,
SPD content of the card should be checked to verify Address Mirroring.
for UDIMM : Byte 131 (0x083), [value=1 is Mirrored]
for RDIMM/LRDIMM : Byte 136 (0x088), [value=1 is Mirrored]
These values apply to Rank 1 and 3 only.
Generally speaking, if the card has 2 or more ranks, then Rank Mirroring is probably used.
Regards,
Ahmed Noeman