Hello,
I would like to ask 2 questions as below from my customer.
Q1) OSCout1 output condition when OSCout1 is disable
As of now, OSCout1 output is "High" (3.3V) when this signal is disable.
Is this condition correct?
Q2) PLL lock
Now the customer is using this device with "Single-PLL" mode.
In case of "0" delay setting of digital delay, PLL is not locked.
I do not know the reason why PLL is not locked.
Should I set/change something "loop-filter" setting to make PLL work well when delay is 0?
Or something other reason?
I appreciate any advice for these questions.
Thank you.
Takumi