This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04906 OSCin spec

Other Parts Discussed in Thread: LMK04906

Per spec, the max OSCin frequency of LMK04906 should below 500MHz. But is there a minimum input frequency? If the input frequency is 5KHz, will it work?

  • Hi Yang,

    In theory, 5 kHz on OSCin should be work since VCO (min) / (max VCO Divider * max N2 Prescalar * max N2 divider) is < 5 kHz. It is however important that the slew rate and amplitude requirement for OSCin on Page 11 of the datasheet are met.

    Regads

    Arvind Sridhar