Other Parts Discussed in Thread: LMK04000
LMK04000 family's evaluation board schematic picture is not clear to see component How can I find clear picture of EVB schematic and second question is there are two ref. clock in(CLKin0/CLKin1) for lmk04033b..should I excite this two ref clocks to create clock signal in output clocks or VCXO crystal is enough and if I should use what would be the best option for this two ref clock in.... I dont use Fout port of LMK04033b...should I left empty or terminate with 50 ohm or what is the best option for Fout port
regard
Edward