Hello everyone I have few question about the lmk04033b. I will use 20 MHZ cyrstal osc for OSCin ports. Should I use another crystal oscillator for CLKin0 and CLKin1 ports and if I excite these two port with same oscillator which is factor of 20 MHZ crystal osc. is this ok for the lmk04033b. in evaluation board schematic there are two Loop filter design for PLL2 Loop filter if I use crystal osc. should I remove VCXO loop filter circuit in my design.
Thanks in advance