This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04906 output clock issues

Other Parts Discussed in Thread: LMK04906, CODELOADER, USB2ANY

I've recently purchased a LMK04906 Evaluation Board (2011-12-06 v1.0).  However, I'm unable to operate the board and generate an output clock despite my best efforts.

I've followed the User's Guide closely with my board and the program CodeLoader (program version: 4.9.0; part file version: 2013-08-19, v1.2).  As soon as a 5.0 V power supply is connected to the Vcc input on the board, I observe a 25 MHz square wave at CLKout3 and CLKout3* and a 95 MHz square wave at CLKout4 and CLKout4*.  The rest of the outputs have no signal.  I then connect a 125 MHz square wave to the FBCLKin*/CLKin1* input on the board.  After repeating the User's Guide's steps, I'm unable to change any of the signals I see from the outputs.  I would appreciate any and all help in getting my eval board up and running as soon as possible.

Please note that the LED 'D4' was red, as expected, during my tests.  Also note that I'm using your USB2ANY adapter to connect the eval board to my PC running Windows 7.  The signals were observed using an Agilent Technologies InfiniiVision MSO07104 Oscilloscope with a 50 Ohm impedance.  The 125 MHz input clock was generated using a Picosecond Pulse Labs Model 12020 1.6 GHz Pulse/Pattern Generator which has a 50 Ohm impedance.  I have taken photos, screenshots, and scope traces detailing what I've done and observed.  This supporting documentation has been compiled into a PDF which is attached to this post.

Steps to recreate the problem:

1) Connect 5.0 V from power supply to Vcc input on eval board

2) Connect 125 MHz square wave from pulse generator to FBCLKin*/CLKin1* input on eval board

3) Open "CodeLoader 4" program on PC running Windows 7

4) In the "Port Setup" tab, select "USB" radio button in "Communication Mode" section

5) In the "Pin Configuration" section, set the Clock Bit to 8, Data bit to 4, LE Bit to 2, SYNC to 1, Status_CLKin0 to 9, Status_CLKin1 to 3, and TRIGGER to 10

6) In the menu bar, select "Select device" > "Clock Conditioners" > "LMK0406B" (and press Control-L)

7) In the menu bar, select “Mode” > “125 MHz CLKin1, 25 MHz VCXO” (and press Control-L)

8) In "Clock Outputs" tab, select "Powerdown" checkbox for CLKout1, deselect "Powerdown" checkbox for CLKout2, and set Clock Output to "LVCMOS (Norm/Norm)" (and press Control-L)

9) In "Bits/Pins" tab, set CLKin1_BUF_TYPE to "MOS" in "CLKin" section (and press Control-L)

LMK04906_Problem.pdf
  • Hi David,

    A quick check to see if communications with the EVM is working is to toggle the POWERDOWN check box in the Bits/Pins tab. You should see the current on the 5V supply drop - can you confirm this communication link is working? I assume the LED on the USB2ANY flashes when the identify button is pressed as well.

    Also, there is no need to change any of the Pin Configuration bits other than the Status_CLKin1 bit to Pin 3 (this should not affect the functionality of the device).

    Gabe

  • Hi Gabe,

    Thank you for your response.  I probed the eval board while toggling the "POWERDOWN" check box in the "Bits/Pins" tab as you suggested, and I could not observe any difference in my measurements.  I too suspect that there is a bad connection link.  The LED on the USB2ANY box does indeed flashes when I click the "Identify" button.

    I went ahead and just ordered another LMK04906 eval board.  This one appears to work straight out-of-the-box (see attached PDF).  When I repeat the identical steps I mentioned in my original post, the 'D4' and 'D5' LED light up red and green, respectively.  On the original board, I never saw the 'D5' LED light up green.  In any case, this new board changes it's output behavior in response to changes in the CodeLoader interface, as expected.

    David

    LMK04906_Problem_Update.pdf
  • Hi David,

    Let's continue this discussion offline. Please send me an email at g-ayala@ti.com.

    Gabe