Hi,
I encountered some problems , When I useed lmk04808.
My system:
Mode : Dual Loop Mode
clkin0 : 125M (lvpecl)
clkin1 : 125M (lvpecl)
output : 125M (lvpecl)
PLL1_R : 125
PLL1_N : 125
My configuration:
R0 = 0x000002E0
R1 = 0x000002E1
R2 = 0x800002E2
R3 = 0xC0000023
R4 = 0x40000024
R5 = 0x000002E5
R6 = 0x24440006
R7 = 0x22220007
R8 = 0x22440008
R9 = 0x55555549
R10 = 0x91C0400A
R11 = 0x03F0300B
R12 = 0x830C016C
R13 = 0x1B13106D
R14 = 0x130FC00E
R15 = 0x0000004F
R16 = 0x01550410
R24 = 0x000000D8
R25 = 0x00410019
R26 = 0x8FA8001A
R27 = 0x1C001F5B
R28 = 0x00201F5C
R29 = 0x010002FD
R30 = 0x010002FE
R31 = 0x001F003F
My issue:
PLL1 sometimes locked and sometimes not locked.
When it not locked ,I found PLL1_R/2 is a DC signal(3.3V), and the signal input clkin0 is correct, clkin0_los is low.
when power on the chip , if temperature is greater than 35℃(Approximation) , PLL1 always can not lock.
If temperature is less than 35℃(Approximation) , PLL1 usually locked, and once locked PLL will remain locked.
How to solve this problem?
Thanks and Best Regards