Hi,
I have a question about clock IC.
I'm searching for the clock buffer which support "clipped sine wave" input from TCXO.
Is there any TI clock buffer IC which support the following:
/////////////////////////////////
*TCXO clipped sine wave input
*3 output
*output level : LVPECL or CMOS
*Max 27MHz output
/////////////////////////////////
It seem there are no TI clock buffer which matches.
Therefore, I wonder if the following TI clock generator can be the solution:
///////////
*LMK03806
*CDCLVC1310
///////////
Is it available? If not which TI clock IC can be used for my request?
best regards,
g.f.