Hi,
My customer is using CECD937 but now the customer is considering to use CDCE925 instead of CDCE937 due to small PKG. Is this possible to replace?
As of now, the specifications of the customer are as follows. (By using CDCE937)
Input : 27MHz,
Output : 37.125MHz, 27MHz, 12MHz, 24MHz, 48MHz
Is this possible for CDCE925 to produce these clocks with same performance as CDCE937?
Or if you know better device than CDCE925 (smaller PKG size, better performance), please let me know.
Thank you very much for your support in advacne.
Best Regards,