Other Parts Discussed in Thread: CDCM1802, LMK00306
Hello,
My customer have some questions about CDCM1802.
They want use CDCM1802 with LVDS input.
[Q1]
Input voltage swing between IN and _IN is listed as follows.
(A) VIN (Input voltage swing between IN and _IN, See Note 1) = 500mV(min), 1300mV(max)
*Note 1 : Is required to maintain ac specifications
(B) VIN (Input voltage swing between IN and _IN, See Note 2) = 150mV(min), 1300mV(max)
*Note 2 : Is required to maintain device functionality
I think the specification of LVDS input is (B). Is it right ?
[Q2]
In the case of LVDS input, are there ac specifications to degrade ?
What are the specifications ?
Do you have some data how much deteriorates ?
[Q3]
Should they assume it LVPECL input?
Best Regards,
Hiroshi Katsunaga