The application intends to use CDCLVC1103 Clock Buffer. What is the Cload of each output pin for this specific clock buufer?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The application intends to use CDCLVC1103 Clock Buffer. What is the Cload of each output pin for this specific clock buufer?
Hello,
Cload describes the receiver input load capacitance.
The CDCLVC110x Familiy is designed to drive typically up to 8 pF load at each output. Higher loads will decrease the signal slew rate. Best performance is achieved with Cload < 5pF.
Best regards,
Julian
Hello Santhosh,
the typical Cin for the CDCLVC110x family is ~2pF.
Best regards,
Julian