Other Parts Discussed in Thread: LMK04828
I need to Synchronize multiple LMK04828 devices (~100 devices/cards) being clocked at ~400MHz. MY REFCLK output from each card would be ~1200MHz. I need a consistent phase relationship between all devices, SYNC to SYNC, for beam-steering a phased array! The 100 cards themselves can be ~20 meters between one another. The problem I'm trying to get my mind around is the varying amount of jitter in long LVDS cables runs for a SYNC signal fan-out. Has anyone out there dealt with a similar issue and came up with a nice solution?