Hello,
The datasheet mentions that LVCMOS_CLK Vih range is from 2V to VDD+0.3V.So I understand it could be 2.5V.
Regarding CLK input, when it is being used as a LVCMOS single ended input, there is unclarity about it's Vih.The datasheet refers only to it's differential input characteristics and Vin=3.465V.
The question is can both LVCMOS_CLK and CLK inputs use Vih=2.5V?
Best Regards,
Tania Bercovich.