Other Parts Discussed in Thread: LMX2531, CODELOADER
Dear TIer,
I want to utilize matlab to automatically sweep the output of LMX2531 from 1.5GHz to 2.5GHz.
Is it available ? If yes, please let me know how to control .
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMX2531, CODELOADER
Dear TIer,
I want to utilize matlab to automatically sweep the output of LMX2531 from 1.5GHz to 2.5GHz.
Is it available ? If yes, please let me know how to control .
Thanks.
Hi Avraka,
Although this is possible with any SPI master device capable of interfacing with MATLAB, we do not natively support this feature. You could leverage Codeloader to generate the appropriate register maps which would then need to be sent to the device via your custom MATLAB/SPI interface.
Codeloader does feature ActiveX functionality which could also be leveraged by MATLAB. More instructions on the ActiveX portion of codeloader can be found on the product page.
Gabe
Hi
i want to control board using matlab.
i don't find board that is frequency synthesizer and other boards
our specs,
output signal: 1500 MHz ~ 2000 MHz.
control output signal(sweep function) ex step is 1 MHz
only i want to have output signal.
thank you.
I'm not quite sure I understand your request. I'd recommend using CodeLoader to generate an appropriate register map. Then you can interface MATLAB with a SPI master to control the LMX device.
Gabe