I setup ClockPro 1.2 without EVB (lockal mode). I can't choose cdce706 in View Setup winwow
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Alex,
that is correct. The performance EVM of the CDCE706 has a parallel port and can only be used with this software. Clock Pro is used for the programming EVM (socket-based EEPROM programmer). You can access the menu for that using the button when the software starts up or in the top menu bar "Tools/Programming EVM".
Best regards,
Patrick
Hello Alex,
for creating a register configuration you will need this software http://www.ti.com/lit/zip/scac073.
The Programming EVM Tool feature of Clock Pro works when you connect an EVM and you have a device inserted.
Best regards,
Patrick
Hi Patrick,
I have the same question with Alex, so I download the software http://www.ti.com/lit/zip/scac073 and install it, there is error when I install the software. It show that "Unable to local the LabVIEW Run-Time Engine", need to contact the vendor. Please find the detail as attached.
Regards,
Nanfang
Hello Nanfang,
you will need a Labview Runtime Engine 8.2x. When you are on Windows operating system this should work for you: http://www.ni.com/download/labview-run-time-engine-8.2.1/550/en/.
Best regards,
Patrick