Other Parts Discussed in Thread: LMK02002, LMK02000, LMK01000
I intend to use LMK02000 to divide a 125MHz to 200MHz signal by 510. However the output oscillates with multiple tones > 50MHz, when the input frequency is below 320MHz. My supply voltage is 3.3V. I have also tried LMK02002 but the behavior is same.
Also I would like to know the expected behavior of the chip when the part is programmed but no input is applied.
My experiment setup is as follows
1) OSCin input is not connected. 2) Fin is driven single ended with Fin* bypassed to GND with 0.1uF 3)LDO bypass and bias pins decoupled as recommended 4) ClKout4 terminated with resistors (127 ohms to VDD and 82 Ohms to GND) 5) All other pins left floating 6) Program R0 with "80 00 00 00" 7) Program R4 with "00 03 FF 04" (Or other division ratios) 8) Program R14 with "2A 00 FF 0E"