Other Parts Discussed in Thread: CDCM7005, CDCM7005-SP
4111.CDCM7005.zipHello
I wold like to ask you to review the below
My cusotmer is testing CDCM7005 and she is facing with PLL Unlock problem and the below are staus for setting values. What are different things between them
================ Below =========================
1. Ref clock: 10MHz VCTCXO
2. VCXO Clock: 44.8MH
3. Register - UNLOCK
Word 0 : 0x00002004
Word 1 : 0x00002001
Word 2 : 0xd0c014a2
Word 3 : 0x00000027
As above the setting Values, they are UnLock.
Therefore, I changed register for PLL Lock but it is still unstable.
4. Lock status but unstable
Word 2 : 0xd0c014aa : PRECP => 1
Word 3 : 0x0000002f : Lock Window : Cycle slip
===========================================================
Thanks