Other Parts Discussed in Thread: LMK04821
In the design example of the LMK04821 datasheet, it is stated that:
"In this example, the 245.76 MHz ADC output needs the best performance. DCLKout2 on the LMK0482x provides the best noise floor / performance. "
In addition to this, most performance charts for high-speed clocking seem to deal with DCLKout2 and DCLKout0.
My question is: Are the DCLKout0/2 outputs better in some way than the other DCLK outputs for accurate clocking of high-speed data converters? If so, is there some part of the datasheet that I have overlooked which provides details on these differences?
Thanks and best regards,
Daniel