Other Parts Discussed in Thread: LMK04821
The electrical characteristics of the LVDS outputs in the LMK04821 datasheet note "AC-coupled to receiver input" as a test condition. Additionally it mentions in a small footnote that LVDS needs a "560 ohm shunt". The EVM seems to use a 560 ohm resistor across the differential pair along with AC-coupling capacitors for all LVDS outputs.
Question 1: Is DC-coupled LVDS allowed? We would like to skip the AC-coupling capacitors (to lower the component count/space required) and directly connect the LVDS pairs to 100 ohm terminations in the receiver.
Question 2: If DC-coupling is allowed, will the differential swing and common-mode voltage match the numbers in the datasheet which are only given for AC-coupled output?
Question 3: If DC-coupling is allowed, can we then skip the 560 ohm resistor? Why is the 560 ohm shunt required?
Thanks and best regards,
Daniel