My lab equipment have passed experiment.It will be implemented its product process.In my orignal design,Used lower jitter oscillator as TLK2711Aclock.
The 2711A require single end CLOCK ( frequent jitter < 100ppm, p-p jitter < 40ps).
When used oscillator , I need to try many oscillators.
It canbe accept in lab equipments. But in product process, It can not be accept;
I want to a CLOCK IC,Its inputs did not require precision oscillator. (normal oscillator can work well,jitter tolerance < 200ppm~1000ppm).
Its output can meet 2711A requirments.(80~135MHz,frequent jitter < 100ppm, p-p jitter < 40ps)
In my hope, The Clock IC is can be control easy. Used pulldown or pull up as control is a best control(Non mandatory requirements)
Can provide a solution?