Hi:
I want to use de CDCLVC1104 as a buffer for the clock signals that 2 ADC will recive from the same source...
I've read the datasheet, and in the "application" section 10.2 it uses a 50-Ohm trace before the CPU clock... Is this valid for ADC? the adc im using is PCM3168.
And how can i achieve that 50-Ohm trace? should i make PCB traces long for that? cause that makes me waste space.
And what happens if my PCB trace has much less than 50 Ohm? is there a problem or the datasheet just states one example?
I've read it but i don't find much clear... Is the first time i use buffer for clock
Can someone send me a refference design of how using the CDCLVC1104 pleas?