I am trying to cascade two timers to produce a 33KHZ burst. 1ms pulse width 10ms rep. The application is for an IR emitter and a proximity sensor with an Automatic Gain Control circuit. The first timer is designed for Astable operation to produce the 33KHZ signal that's done the problem is feeding that signal in to the 2nd cascaded timer. What I have done to date is to design using Monostable operation, and according to the data sheet I selected the RA to be 1M Ohm and C is .01uf and I also used C= .1uf. My output rep rate is 10ms which is what I am looking for however when I expand the pulse its a 12us pulse, I need that pulse to be 1ms. If I change RA to give me a 1ms pulse width, I loose the 10ms rep rate. I may not have this configured correctly, can you help me with this problem. All I am trying to do is to cascade of two 555 timers to generate a burst pattern at 33kHz signal for 1ms, an OFF period for 10ms. Thank you.