I have a customer switching to the LMX2581 for his new product. He previously had used the LMX2541. He has found in the datasheet that the input Osc levels are different between the two parts. It would appear he needs 400mV pk-pk minimum on the LMX2581 input. The LMX2541 only needed half of this. The problem here is that he has an LVDS source which is typically 400mV, but can vary a bit below that by spec. His input frequency is 368MHz. We don't want to add a buffer since that will add phase noise which we can't afford.
Are we trying to say that this part can't take an LVDS input ?? That would seem strange to me... I hope not.
I also see Figure 12 in the datasheet that suggests we don't really need 400mV pk-pk. It shows -23dBm sensitivity at 368MHz.
Can he use an LVDS input ??
thanks,