Hello. I use CDCE72010 on our boards. On some of them, there is 1.2ns additional delay on the random output after outputs were synchronised. Others boards are OK, all outputs are synchronised correctly. This additional delay is independent on the output divider settings or method of synchronization (external RESET pin or via SPI registers) and delay is the same on the boards with this behavior. Please has anybody the similar experience and found the solution. Thank you. Best regards, Pavel Subrt