I am looking into using the LMK01000 evaluation board for some testing requirements. I see that the User's Guide discusses two options for programming the device. Either a computer with a parallel port and Windows XP, or a USB2ANY-uWIRE interface. I looked to see if I could find the USB2ANY-uWIRE interface and I couldn't find any additional information on this. Is the USB2ANY-uWIRE option really available for programming this device? If I purchase the eval board does it come with the USB adapter board? Is the only option available to program the device on the eval board a PC with a parallel port?
Thanks,
Dave