Hi,
In the datasheet,
Vcc=0V, Vee=-2.375V to -3.8V, Iee=min 45, max 82mA, Icc=max 370mA.
If use 6ch of 10ch, how can I calculate power consumption?
Do I have to do Iee+Icc*6/9?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In the datasheet,
Vcc=0V, Vee=-2.375V to -3.8V, Iee=min 45, max 82mA, Icc=max 370mA.
If use 6ch of 10ch, how can I calculate power consumption?
Do I have to do Iee+Icc*6/9?
When 6 loaded outputs (and 4 unused outputs unloaded/open), the total supply current from the positive power supply is as follows:
Isupply = Iee_max + (Icc_max - Iee_max)*(6/10)
The total power (Isupply * Vs_max) will be dissipated in the device and output load resistors. You can estimate output load power to be ~50mW/output pair. To get the device power consumption, subtract total load power from the total power.
Regards,
Alan