Hi,
We are considering replacements for SY89846UMG. It has isolation not to interfere each clock.
Is there 2:1 differential input multiplexer with Fail-Safe input protection ?
Best Regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are considering replacements for SY89846UMG. It has isolation not to interfere each clock.
Is there 2:1 differential input multiplexer with Fail-Safe input protection ?
Best Regards,
Kato
Foffset is the offset frequency between the selected input (victim) and the non-selected input (aggressor). For example, if Fclkin0 = 100 MHz, then Fclkin1 = 100 MHz +/- 50 kHz (or greater). We needed offset to be >50 kHz so the crosstalk sideband spur power level due to the aggressor input is clearly seen above the noise skirt of the measured fundamental output signal for the selected input.
PclkinX is the reference input power levels used for the aggressor and victim inputs (both 0 dBm ). If the aggressor input power level is increased relative to the 0 dBm reference, then the ISOmux spec should increase (get worse) by the same amount in dB. For example, for CLKin0 = 100 MHz, 0 dBm (victim) and CLKin1 = 101 MHz, +2 dBm (aggressor), the input mux isolation would become -82 dBc (=-84 dBc typ spec + 2 dB aggressor power above 0 dBm reference levels).
To translate the ISOmux spec (i.e. phase spur power level, in dBc, induced by input mux crosstalk) to the equivalent "Crosstalk-Induced Jitter" spec, you can use the same formula as phase spur level induced by power supply noise (referred to as "PSRR" in the datasheet).
Deterministic Jitter (peak-to-peak) due to periodic noise signal:
DJ p-p = 2 * 10^(-|dBc|/20) / (pi * Fclk), where dBc is a single-sideband spur power level relative to carrier measured at the output induced by a single fundamental noise signal like power supply ripple or input mux crosstalk.
DJ p-p can be expressed as RMS value as shown below.
DJ rms = DJ p-p / (2 * sqrt(2))
SAMPLE CALCULATION:
For the ISOmux spec = -84 dBc @ Fclkin=100 MHz, Foffset>50kHz, Pclkin=0dBm conditions, this results in DJ = 0.4 ps p-p, or DJ = 0.14 ps rms.
Regards,
Alan
Hi Alan - san,
Thank you for the detailed explanation. I was very understanding. By the way, could you provide the Mux Isolation evaluation results ? If possible, could you provide the data of fclkin=622.08MHz(LVPECL) for LMK00304 ?
Best Regards,
Kato