This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

multiple output Clock generator evaluation module

Other Parts Discussed in Thread: LMK04828, LMX2581, LMK04808

Hi,

I am looking for a clock generator which generates  200Mhz to 3GHz LVDS output (multiple outputs) module with less jitter.

Please suggest me the evaluation boards which TI supports.

This module i will use to drive the multiple DAC modules, so please let me know weather these outputs has any phase delays.

Thanks & Regards,

Krish

  • Hi Krish,

    LMK04828 in single-PLL (PLL2 only) mode is one option but the limitation is that PLL2 is an integer PLL. 

    Another option is LMX2581 (Frac-N PLL) which can generate a single frequency that can then be buffered with a device like LMK04808 (in Clock distribution mode)

    LMK048xx parts support analog and digital delay adjustment on the output clock and can support LVDS

    Regards

    Arvind Sridhar