This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF3765: External VCO input to outputs frequency response (no PLL)

Other Parts Discussed in Thread: TRF3765

we would like to use the external VCO input to optionally distribute an external clock that can be > 4800 MHz to the TRF3765 outputs. In a prior case Mr. Hanish said....

Analog blocks do not exhibit these hard limits and tend to roll off functionality softly. For example, the electrical characteristics table in the datasheet describes a 9GHz limit where power output has rolled off by 20dB compared to normal, in-band levels.

http://e2e.ti.com/support/rf__digital_radio/high_performance_rf_modulators_pll_and_vco_products/f/224/t/219816

Is there more insertion loss information (plot, -3 and/or -6 dB bandwidth perhaps) and am I correct in that the TRF3765 can be used as a distribution buffer from the external VCO input?

many thanks

Dave