Hello,
I'm trying to use a LMX2581EVM and had a query regarding the output power level. The datasheet mentions that for an output frequency of 2.7GHz, an inductive pull up gives an output power varying from about roughly 7dBm to 12dBm.
With RFoutA powered down using software, using RFoutB of the EVM, which has a 18nH inductive pull up, the output power for me varies from 3.7dBm to 9.5dBm. The unused output is terminated with a 50 ohm resistance. My concern is why the output power level is only 3.7dBm for a setting of 15 as OUT_PWRB. This is because, that setting gives be the best phase noise performance but not sufficient output power (7dBm would work for my application). What could be the reason for this and how can I improve it? (I am aware of the fact that the pull up components are not placed close to the output on the EVM, however would this result in such a large drop in the output power?)
Also, while RFoutB+ and RFoutB- give similar output power, RFoutA+ and RFoutA- tend to have slightly varying power levels. Additionally, what type (resistive/inductive) of pull up would be better in terms of the phase noise performance?
Another query I has was in the LMX2581 EVM, using the internal XO, what is the peak to peak voltage swing at the OSCin pin?
Awaiting a reply,
Thanks and Regards,
Ajay