I just received the LMX2571 Eval board and USB2ANY. I downloaded the current version of CodeLoader and installed it. The first time I plugged in the USB2ANY it wanted to update firmware. I acknowledged and it tried to download, but stated it failed after a few minutes. I repeated the process and it again asked to update firmware. I again agreed and it started and then stopped. I waited about 15 minutes after Windows XP showed that Codeloader was not responding and forced quit.
When I launch CodeLoader it seems to run on XP, but there is no indication that it is talking to the USB2ANY box. The "USB" radio button is grey and the "Identify" button is grey as well. I've also installed CodeLoader on a Windows 7 machine. Again, CodeLoader appears to run, but will not talk to the USB2ANY.
My guess is that firmware did not successfully update, but this is only a guess.
HELP!!!! How can I get this USB2ANY to function?
Thanks.