Hi,
I would like to change the clock frequency as I want after the system begins running. Can I configure it in pin programmable mode?If yes, could you recommend a hardware configuration.
Or, I can only achieve it by SPI or I2C mode.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to change the clock frequency as I want after the system begins running. Can I configure it in pin programmable mode?If yes, could you recommend a hardware configuration.
Or, I can only achieve it by SPI or I2C mode.
Thanks.
Hi,
Programming via I2C/SPI is not available in Pin Mode. In Pin mode, the state of the control pins determines the configuration of the device for all device states. Pages 36-41 of the datasheet has information on supported configurations in Pin Mode.
Regards
Arvind Sridhar