Hi All,
I plan to use the CDCLVC1104 to fan out an MDC clock signal on my PCB. The chip receiving the clock uses a 2.5V swing so I was planning to power the CDCLVC1104 with 2.5V. The clock signal that is being provided from of board has a 3.3V swing. My question is, can the CDCLVC1104 accept the 3.3V swing input while being powered at 2.5V? Or another way, when powered with 2.5V is the CDCLVC1104 3.3V tolerant?
Thank you,
Michael Nycz